""
Marine

Gladding-Hearn Delivers Calcasieu Pass Pilot to Lake Charles Pilots

by Alan Haig-Brown

Cummins Vessel Reference #588

Photos courtesy of Gladding-Hearn Shipbuilding: The pilot boat Calcasieu Pass Pilot at speed on calm waters.

 

In America, deep-V hulls are synonymous with the late C. Raymond Hunt who founded the firm with current president John Deknatel in the 1960s. The Deep-V hull has been a mainstay of the company ever since. According to the company web page, www.huntdesigns.com the design was, “Conceived and patented by C. Raymond Hunt in 1963, the high-deadrise, or deep-V, hull is proven and accepted as the ultimate hull form for speed with comfort and safety in rough water. … The sharp entry forward keeps pounding to a minimum. There is no deep forefoot to cause bow steering and broaching. The V-shape is carried all the way to the transom, which results in evenly distributed displacement and lateral plane….”

 

 

 

The control console on the new Lake Charles pilot boat.

 

Since 1978 C. Raymond Hunt Associates have collaborated more than 40 times with Gladding-Hearn Shipbuilding to design and build tough, high-speed deep-V pilot boats. As ship draft has increased pilots have moved further off shore in meeting ships and often board at higher speed. The collaboration of designer and builder has, over the years, evolved a range of pilot boats designs to meet a range of requirements, from the 43-foot Resilient Class to the 75-foot Charleston Class. It was this later hull that formed the basis on which the Lake Charles pilots worked to develop a boat to meet their own particular needs. www.gladding-hearn.com/

 

Designed by C. Raymond Hunt and built at Gladding-Hearn, the new 75 by 20.6-foot (waterline 67’11”) boat has been delivered to the Lake Charles pilots. The vessel is powered by a pair of Cummins QSK38 Tier 2 engines each developing 1350 HP at 1900 RPM and turning 5-blade 41-inch Bruton props through quick shift Twin Disc MGX-6620A gears. The Twin Disc MGX-6620-A gears have a 10-degree down angle to the propeller shaft allowing the engines to be mounted well aft in the hull and at an angle of only four degrees while keeping the propellers deeper in the water for maximum bite.

The Tier 2 main engines on the pilot boat are fitted with the Cummins Eliminator oil lube filtering systems. These replace disposable filters with self-cleaning centrifuges that reduce maintenance expense and improve engine life. Cummins Northeast Inc also supplied two Cummins Power Generation-Onan 27.5 kW marine generator sets.

 

 

One of the two Cummins QSK38 Tier 2 engines being installed.

 

With these engines, the C. Raymond Hunt designed, Gladding-Hearn built and Cummins-powered 75’8”x20’8”x10’ Lake Charles pilot boat reaches speeds of 25.9 knots fully loaded and 27 knots light boat.

 

 

For further information:

 

Peter Duclos
Gladding-Hearn Shipbuilding
Duclos Corp.
1 Riverside Ave.
Box 300
Somerset, MA 02726
Phone: 508 676 8596
Email: [email protected]

Cheryl P. Lavalley, P.E.
Cummins Northeast, Inc.
Distributor Application Engineer, Industrial & Marine
Phone: 781 751 1273
Email: [email protected]

Capt. Mike Miller,
President
Lake Charles Plots
4902 Ihles Road,
Lake Charles, LA70605
Phone: 337 436 0372
Email: [email protected] | [email protected]
Website: lakecharlespilots.com

Winn Willard,
Vice_President
C.Raymond Hunt Associates
5 Dover St. Suite 105
New Bedford, MA 02740
Phone: 508 717 0600
Email: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...