How AI is shaping the future of data center power infrastructure design

By Cummins Inc., Global Power Technology Leader

How AI is shaping the future of data center power infrastructure design

The insatiable appetite for data in our digital world is forcing a reassessment of the way data centers are designed, built, and operated. 

The power crunch—intensified by the colossal energy demands of AI—is stretching the existing data center infrastructure to its limits.

Cummins Power Generation is working in lockstep with the data center sector to provide power solutions that can address the high intensity and unpredictable fluctuations associated with AI.

What is the most common rack density range in data centers?

The most common rack density range, according to Uptime Institute's Global Data Center Survey 2025, is 5-9 kW per rack. The figure has remained fairly constant over the past five years, and is a long way short of the widely predicted surge to 20kw+ for the industry in general.

Still, Uptime expects rack densities will rise steadily over the coming years as more data centers adopt servers in the 10kw-30kw range.

The big question for data center operators will be whether their existing infrastructure can handle the future capacity and power demands of upcoming hardware generations, like new NVIDIA GPU systems, or if they even want to go down that route knowing it will be hugely expensive.

The introduction of Nvidia’s Blackwell GPUs and GB200NVL72 rack designs in 2024 saw peak rack power density rise to132 kW, and future models like Blackwell Ultra and Rubin AI servers will require between 250 and 900 kW, with up to 576 GPUs per rack by 2026-2027.

Top-end AI servers are projected to break through the mythical 1MW barrier with the arrival, slated for 2028, of Nvidia’s Rubin Ultra AI GPU and HBM4 memory.

Such advancements are underscoring the expansion of data center campuses from tens of megawatts to hundreds of megawatts, with some planning for gigawatt-scale power consumption.

Large investments in data centers

At the recent Pennsylvania Energy and Innovation Summit, several major players in data center and energy infrastructure announced huge and symbolic investments:

Blackstone and PPL Corporation announced a $25B joint venture investment to develop natural gas-fired plants tailored for data center needs; CoreWeave is launching a $6B data center project to meet GPU/AI demand; Google and Brookfield Renewable are working to secure 3GW of hydro power to ensure sustainable supply for their infrastructure; and Amazon Web Services (AWS) will spend $20B on two data center complexes in Pennsylvania, including one it is building alongside a nuclear facility with the idea that it will essentially plug directly into the power plant.

Picking up the nuclear theme, engineering giant Rolls-Royce is confident the small modular reactors (SMRs) it builds for nuclear submarines can be adapted to play a role in the data center business, notwithstanding concerns over the supply of water for the reactor’s cooling systems.

With major data center operators recognizing the gargantuan need for power for the AI ecosystem, the next challenge becomes how to deliver that power to the servers demanding it.

Higher Voltage results in more computing density

In a conventional data center setup, AC power is converted to DC, and from that point there can be multiple DC-DC conversions (ie 300V down to 48V). At each conversion point, energy is lost and heat generated, increasing operational costs and environmental impact.

Centralizing the rectification process means converting AC to DC closer to the source, then distributing high-voltage DC directly to the racks, reducing losses and boosting Power Usage Effectiveness (PUE).

It is widely anticipated hyperscalers like Meta, Google and Microsoft will move to deploy medium voltage (MV) distribution – up to 13.8kV – and higher DC voltage 400VDC and 800VDC architectures to take advantage of the greater power density of AI server racks.

With the lower currents required, they can expect to recover huge amounts of previously lost energy while enjoying significant savings in the amount of copper needed for cabling.

Moreover, HV architecture also allows for more power to be delivered in a smaller physical footprint, freeing up precious rack space and increasing the computing density of the data center.

While companies like NVIDIA are driving the development of new ecosystems for 800VDC, there is a need for a wider range of commercially available hardware, including solid-state transformers (SSTs), high-efficiency DC-DC converters, and specialized power shelves.

Cummins partners with hyperscalers

Cummins is busy on several fronts helping the data centre sector navigate the world of AI-driven power demand.

In partnership with one of its major hyperscaler accounts, Cummins is creating modelling systems for its generator sets that can calibrate against actual live AI workloads, providing much-needed clarity and confidence.

Cummins is also studying the market and talking to manufacturers about solid state transformer (SSTs), which can precisely regulate voltage while integrating seamlessly with both AC and DC systems. One of the key advantages of SSTs is they can take MV distribution from the grid and convert it directly to DC power. Also, as they are far smaller and lighter than a comparable core-based transformer, SSTs offer data centers enhanced scope on design and layout.

A report from the Compound Semiconductor Applications (CSA) Catapult predicts the market for SSTs will grow at a double-digit compound annual growth rate through to 2030, driven by the rapid expansion of renewable energy, EV charging infrastructure and smart grid upgrades.

For greater operational flexibility, data centers can disconnect from the grid and run entirely on their onsite assets. Cummins is supporting this strategy by developing tier 4 diesel and natural gas generators, battery energy storage systems (BESS), and microgrid deployment capabilities, allowing operators to use onsite assets to build out their data centers where grids are constrained.

At its Power Integration Center in Fridley, Minnesota, Cummins is configuring, testing, and validating a range of microgrid power systems, including diesel and natural gas gen-sets, photovoltaic solar, battery storage, fuel cells, and transfer switches.

Cummins has also recently introduced two fully containerized Battery Energy Storage Systems (BESS) solutions which can harvest energy during off-peak hours (when electricity is cheaper) and discharge it during peak demand periods. The systems use lithium ferrophosphate (LFP) batteries, renowned for their high cycle life and safety, and span 200kWh to 2MWh capacity.

A BESS transitions from standby to full power in milliseconds. This rapid response provides a seamless, uninterrupted power supply. The BESS can also help stabilize frequency and voltage, mitigating the effects of volatile AI workloads.

BESS can prevent the generator from constantly starting and stopping or running inefficiently at low loads, reducing wear and tear on the engine. This leads to fewer maintenance requirements and extends the overall lifespan of the generator, which lowers long-term ownership costs. As an added benefit, it can dramatically reduce noise pollution, a major advantage for data centers near residential areas.

Cummins' advancements in natural gas reciprocating engines are making them an increasingly competitive option, with the promise of cleaner emissions, quieter operation and lower, more stable fuel costs when connected to a pipeline.

How to partner with Cummins for data center solutions

If you are seeking a trusted partner to help you develop and implement advanced power solutions for the AI era, we would love to have the conversation. Visit https://www.cummins.com/generators/data-centers and use any of the contact buttons to connect with your local distributor.

Author Profiles

Cummins Office Building

Cummins Inc., Global Power Technology Leader

Cummins Inc., a global power leader, is committed to powering a more prosperous world. Since 1919, we have delivered innovative solutions that move people, goods and economies forward. Our five business segments—Engine, Components, Distribution, Power Systems and Accelera™ by Cummins—offer a broad portfolio, including advanced diesel, electric and hybrid powertrains; integrated power generation systems; critical components such as aftertreatment, turbochargers, fuel systems, controls, transmissions, axles and brakes; and zero-emissions technologies like battery and electric powertrain systems. With a global footprint, deep technical expertise and an extensive service network, we deliver dependable, cutting-edge solutions tailored to our customers’ needs, supporting them through the energy transition with our Destination Zero strategy. We create value for customers, investors and employees and strengthen communities through our corporate responsibility global priorities: education, equity and environment. Headquartered in Columbus, Indiana, Cummins employs approximately 67,400 people worldwide and earned $2.8 billion on $33.7 billion in sales in 2025.

Want to find out more?

Receive the latest from Cummins in technologies, products, news, and insights.