On-highway engines
You've got freight to move, deadlines to meet, goals to achieve. We've got a solid history of providing the best, most innovative engine technology to help you get the job done. Cummins delivers the right technology at the right time for you and your operation.
On-highway engine applications
You can depend on Cummins when people are depending on you. Learn more below or request a quote for specialized assistance in specing the exact power you need.
Engineering the next generation of power
Power
330 - 439 hp
Power
246 - 327 kW
Torque
1489 - 1556 lb-ft
Torque
2019 - 2110 N•m
Certification
Euro II,Euro 2
Power
350 - 500 hp
Power
261 - 373 kW
Torque
1328 - 1696 lb-ft
Torque
1801 - 2299 N•m
Certification
Euro V,Euro 5
Power
247 - 316 hp
Power
184 - 236 kW
Torque
730 - 1000 lb-ft
Torque
990 - 1356 N•m
Certification
Euro 6 - Phase D,Euro 6
Power
206 - 395 hp
Power
154 - 295 kW
Torque
1143 - 1260 lb-ft
Torque
1550 - 1708 N•m
Certification
Euro II,Euro 2
Power
220 - 320 hp
Power
164 - 239 kW
Torque
664 - 885 lb-ft
Torque
900 - 1200 N•m
Certification
Euro II,Euro 2
Power
150 - 210 hp
Power
112 - 157 kW
Torque
480 - 627 lb-ft
Torque
651 - 850 N•m
Certification
Euro III,Euro 3
Power
141 - 168 hp
Power
105 - 125 kW
Torque
331 - 442 lb-ft
Torque
449 - 599 N•m
Certification
Euro III,Euro 3
Power
107 - 160 hp
Power
80 - 119 kW
Torque
206 - 265 lb-ft
Torque
279 - 359 N•m
Certification
Euro III,Euro 3
Power
240 - 315 hp
Power
179 - 235 kW
Torque
660 - 950 lb-ft
Torque
895 - 1288 N•m
Maximizing fluid economy in a heavy-duty diesel powertrain begins long before a new truck delivers its first load.
May 18, 2026
Engine nostalgia or not, Cummins’ latest X15 diesel is its most reliable heavy-duty engine yet, improving total cost of ownership for fleets and owner-operators.
February 04, 2026
When shopping for new trucks, experts say fleets and owner-operators should look past the sticker price and focus on the total cost of ownership (TCO).
January 26, 2026
From tough terrain across the United States for UPS to steep grades in Canada, Cummins’ X15N natural gas engine has spent its first year proving it can handle heavy hauls while delivering near-zero emissions at a lower fuel cost than diesel.
December 23, 2025
What if the stuff we throw away could keep trucks moving? In this episode of Power Onward, Kim sits down with Dave to talk about renewable natural gas, aka RNG, and how it turns things like landfill trash, cow manure, and food waste into clean, usable fuel.
November 05, 2025
Fleets that are already using natural gas trucks stand to gain additional value by expanding with Cummins’ portfolio of natural gas engines.
October 24, 2025
Fleets and owner-operators have long known that extending oil change intervals can lead to significant cost savings and environmental benefits.
July 14, 2025
There comes a point when technology can prove less than convenient.
May 07, 2025